FDCAN 1 and FDCAN 2
Good morning, I am currently working on the nuclei H755 ziq. it says on the data sheet and on stm32ide that it has two FDCANS. however, I have only found in the schematics one tx and one rx port. how do I know if they are connected to FDCAN 1 or FDCAN 2? I have found on stm32 side that it was for fdcan 1 and the fdcan 2 on PD15 and PD20. however, it is ,not written on the schematics. is it an error?