Skip to main content
Graduate
March 17, 2025
Solved

fdcan bit time config for classic frame STM32H563VGT6

  • March 17, 2025
  • 1 reply
  • 1229 views

Hi,
this is myproduct code STM32H563VGT6.

I am configuring the FDCAN2 module.
In particular the bit time using the filed below of the init structure of the HAL handler:
hfdcan2.Init.NominalPrescaler (NBRP+1 of register FDCAN_NBTP)
hfdcan2.Init.NominalSyncJumpWidth (NSJW+1 of register FDCAN_NBTP)
hfdcan2.Init.NominalTimeSeg1 (NTSEG1+1 of register FDCAN_NBTP)
hfdcan2.Init.NominalTimeSeg2 (NTSEG1+2 of register FDCAN_NBTP)
The protocol (and the ST manual rm481 at page 2542) specify that TimeSeg1 max value is 16, TimeSeg2 max value is 8.

In the example FDCAN_classic_frame_example I found this values:

hfdcan1.Init.NominalPrescaler = 1;
hfdcan1.Init.NominalSyncJumpWidth = 62;
hfdcan1.Init.NominalTimeSeg1 = 187;
hfdcan1.Init.NominalTimeSeg2 = 62;

Seems that these value are out of range.
I'm definitely missing something.

can someone explain the meaning of the parameters in the example "FDCAN_classic_frame_example" ?

Thank you.

Regards.

    This topic has been closed for replies.
    Best answer by mƎALLEm

    Ah,

    The spec you referred to is for CAN2.0 (bxCAN) not for CANFD (M_CAN/FDCAN).

    Meanwhile, you can use FDCAN peripheral in Classical mode by setting only the nominal bit time. The data phase will be discarded even if you configure it.

    Example provided in CubeH5 for FDCAN configured in Classcal mode: https://github.com/STMicroelectronics/STM32CubeH5/blob/main/Projects/NUCLEO-H563ZI/Examples/FDCAN/FDCAN_Classic_Frame_Networking/

    Hope that helps.

    1 reply

    Technical Moderator
    March 24, 2025

    Hello,

    This is a known issue in the FDCAN spec and it was already internally reported on the ticket 193478. 

    From the reference manual RM481/page 2575:

    mALLEm_0-1742826904410.png

    page 2571:

    mALLEm_1-1742827030540.png

    The correct bit times:

    For Nominal bit time:
    - NTSEG1: between 1 and 256 (* tq)
    - NTSEG1: between 1 and 128 (* tq)
    For Data phase bit time:
    - DTSEG1: between 1 and 32 (* tq)
    - DTSEG2: between 1 and 16 (* tq)

    So the example is correct.


    As you are using Classical frame you need to set only the Nominal bit time.

    Hope that answers your question.

     

    DAUSILIAuthor
    Graduate
    March 24, 2025

    Hi mƎALLEm,
    thank you very much for your reply.

    For Classical CAN I don't understand how max values for NTSEG1 and NTSEG2 can be so high:
    - NTSEG1: 256 (* tq)
    - NTSEG2: 128 (* tq)

    I attach a screenshot from document "BOSCH CAN Specification version 2.0".
    In this document max values expressed in tq are smaller.
    Also "Controller Area Network Konrad Etschberger" book page 82 confirm these limits.

    For sure my fault, but I don't understand.

    Technical Moderator
    March 24, 2025

    Hello,

    I don't know which Bosch spec you get that screen shot from, but you need to refer to the M_CAN.

    This is a screenshot from BOSCH M_CAN spec (page 23):

    mALLEm_0-1742831017690.png

    Hope that answers your question.