FDCAN on Riverdi LCD not send and not received - STM32H757XIH6
Hi all,
For several days I have been trying to send and receive something via CAN, but I am unable to do so on the Riverdi LCD board. I read two posts here with similar problems and instructions and videos from ST, but it did not solve my problem. CAN still does not work in normal mode. I tried too on loopback mode
STM board: >> Riverdi board
On the second board with nucleo 64, I made a simple program that sends 8 bytes and works correctly.

But riverdi board send like this

Now FDCAN set is to 40Mhz and this is code fdcan.c:
void MX_FDCAN1_Init(void)
{
hfdcan1.Instance = FDCAN1;
//hfdcan1.Init.FrameFormat = FDCAN_FRAME_FD_NO_BRS;
//hfdcan1.Init.Mode = FDCAN_MODE_EXTERNAL_LOOPBACK; //I try too
hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan1.Init.AutoRetransmission = ENABLE;
hfdcan1.Init.TransmitPause = DISABLE;
hfdcan1.Init.ProtocolException = DISABLE;
hfdcan1.Init.NominalPrescaler = 1;
hfdcan1.Init.NominalSyncJumpWidth = 10; //ok
hfdcan1.Init.NominalTimeSeg1 = 69;
hfdcan1.Init.NominalTimeSeg2 = 10;
hfdcan1.Init.DataPrescaler = 20; //ok
hfdcan1.Init.DataSyncJumpWidth = 1; //ok
hfdcan1.Init.DataTimeSeg1 = 2; //ok
hfdcan1.Init.DataTimeSeg2 = 1; //ok
hfdcan1.Init.MessageRAMOffset = 0;
hfdcan1.Init.StdFiltersNbr = 1;
hfdcan1.Init.ExtFiltersNbr = 0;
hfdcan1.Init.RxFifo0ElmtsNbr = 1; //ok
hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;
hfdcan1.Init.RxFifo1ElmtsNbr = 0;
hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;
hfdcan1.Init.RxBuffersNbr = 0;
hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8;
hfdcan1.Init.TxEventsNbr = 0;
hfdcan1.Init.TxBuffersNbr = 0;
hfdcan1.Init.TxFifoQueueElmtsNbr = 1; //ok
hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_8;
if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
FDCAN_FilterTypeDef canfilterconfig;
canfilterconfig.IdType = FDCAN_STANDARD_ID;
canfilterconfig.FilterIndex = 0;
canfilterconfig.FilterType = FDCAN_FILTER_MASK; //FDCAN_FILTER_RANGE
canfilterconfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
canfilterconfig.FilterID1 = 0x100;
canfilterconfig.FilterID2 = 0x100;
canfilterconfig.RxBufferIndex = 0;
if (HAL_FDCAN_ConfigFilter(&hfdcan1, &canfilterconfig) != HAL_OK)
{
/* Filter configuration Error */
Error_Handler();
}
HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_REJECT, FDCAN_REJECT, FDCAN_REJECT_REMOTE, FDCAN_REJECT_REMOTE);
}
void HAL_FDCAN_MspInit(FDCAN_HandleTypeDef* fdcanHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
if(fdcanHandle->Instance==FDCAN1)
{
/* USER CODE BEGIN FDCAN1_MspInit 0 */
/* USER CODE END FDCAN1_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_FDCAN;
PeriphClkInitStruct.FdcanClockSelection = RCC_FDCANCLKSOURCE_PLL;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
/* FDCAN1 clock enable */
HAL_RCC_FDCAN_CLK_ENABLED++;
if(HAL_RCC_FDCAN_CLK_ENABLED==1){
__HAL_RCC_FDCAN_CLK_ENABLE();
}
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/**FDCAN1 GPIO Configuration
PB9 ------> FDCAN1_TX
PA11 ------> FDCAN1_RX
*/
GPIO_InitStruct.Pin = GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF9_FDCAN1;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_11;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF9_FDCAN1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* FDCAN1 interrupt Init */
HAL_NVIC_SetPriority(FDCAN1_IT0_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(FDCAN1_IT0_IRQn);
/* USER CODE BEGIN FDCAN1_MspInit 1 */
/* USER CODE END FDCAN1_MspInit 1 */
}
}
And program code:
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "quadspi.h"
#include "myfile.h"
#include "max31855.h"
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#ifndef HSEM_ID_0
#define HSEM_ID_0 (0U) /* HW semaphore 0*/
#endif
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
uint16_t dac_value;
uint16_t adc_value;
char lamik_dane[17];
int16_t temp_int;
//CAN
uint8_t RxData[8];
uint8_t TxData[8];
int datacheck = 0;
enum {tsStop,tsWaiting,tsGetRegisterAddress,tsGetData,tsSendData};
uint8_t DisplayLCD[18];
uint8_t currsorX = 0;
uint8_t currsorY = 0;
uint8_t transferState = tsStop;
uint8_t registerAddress = 0;
uint8_t transmitBuffer = 0;
uint8_t receiveBuffer = 0;
uint8_t DataLength = 0;
uint8_t Data[6];
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
void PeriphCommonClock_Config(void);
void MX_FREERTOS_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
FDCAN_RxHeaderTypeDef RxHeader;
FDCAN_TxHeaderTypeDef TxHeader;
void LED_Init(void)
{
HAL_GPIO_WritePin(GPIOJ, GPIO_PIN_10, GPIO_PIN_RESET);
GPIO_InitTypeDef GPIO_InitStruct = {0};
GPIO_InitStruct.Pin = GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOJ, &GPIO_InitStruct);
}
void HAL_FDCAN_RxFifo0Callback(FDCAN_HandleTypeDef *hfdcan, uint32_t RxFifo0ITs)
{
HAL_FDCAN_GetRxMessage(hfdcan, FDCAN_RX_FIFO0, &RxHeader, RxData);
if (RxHeader.DataLength == 8)
{
datacheck = 1;
strcpy(DisplayLCD,"Recived");
SendToLamik(DisplayLCD);
}
}
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* USER CODE BEGIN Boot_Mode_Sequence_0 */
/* USER CODE END Boot_Mode_Sequence_0 */
/* Enable the CPU Cache */
/* Enable I-Cache---------------------------------------------------------*/
SCB_EnableICache();
/* Enable D-Cache---------------------------------------------------------*/
SCB_EnableDCache();
/* USER CODE BEGIN Boot_Mode_Sequence_1 */
/* USER CODE END Boot_Mode_Sequence_1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* Configure the peripherals common clocks */
PeriphCommonClock_Config();
/* USER CODE BEGIN Boot_Mode_Sequence_2 */
/* When system initialization is finished, Cortex-M7 will release Cortex-M4 by means of
HSEM notification */
/*HW semaphore Clock enable*/
__HAL_RCC_HSEM_CLK_ENABLE();
/*Take HSEM */
HAL_HSEM_FastTake(HSEM_ID_0);
/*Release HSEM in order to notify the CPU2(CM4)*/
HAL_HSEM_Release(HSEM_ID_0,0);
/* wait until CPU2 wakes up from stop mode */
/* USER CODE END Boot_Mode_Sequence_2 */
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_MDMA_Init();
MX_I2C1_Init();
MX_LTDC_Init();
MX_USART1_UART_Init();
MX_I2C4_Init();
MX_DAC1_Init();
MX_DMA2D_Init();
MX_FDCAN1_Init();
//MX_FDCAN2_Init();
MX_SPI1_Init();
MX_TIM3_Init();
MX_TIM5_Init();
MX_TIM6_Init();
MX_UART4_Init();
MX_UART8_Init();
MX_CRC_Init();
//MX_I2C2_Init();
MX_SPI2_Init();
MX_TIM15_Init(); //Podświetlanie PULSE 0-998 MAX TIM15.CCR1 = Your_new_pulse_value;
MX_FATFS_Init();
MX_RNG_Init();
MX_FMC_Init();
MX_JPEG_Init();
MX_RTC_Init();
MX_ADC1_Init();
MX_ADC3_Init();
MX_TouchGFX_Init();
/* Call PreOsInit function */
MX_TouchGFX_PreOSInit();
/* USER CODE BEGIN 2 */
if (BSP_SDRAM_SingleTest() != 0)
{
// Error_Handler();
}
if (CSP_QUADSPI_Init() == HAL_OK) {
CSP_QSPI_EnableMemoryMappedMode();
}
if (HAL_TIM_PWM_Start(&htim15, TIM_CHANNEL_1) != HAL_OK)
{
/* PWM Generation Error */
Error_Handler();
}
LED_Init();
if (HAL_TIM_Base_Start_IT(&htim3) != HAL_OK)
{
/* Starting Error */
Error_Handler();
}
if (HAL_FDCAN_Start(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
if (HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK)
{
Error_Handler();
}
TxHeader.Identifier = 0x10;
TxHeader.IdType = FDCAN_STANDARD_ID;
TxHeader.TxFrameType = FDCAN_DATA_FRAME;
TxHeader.DataLength = FDCAN_DLC_BYTES_8;
TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
TxHeader.BitRateSwitch = FDCAN_BRS_OFF;
TxHeader.FDFormat = FDCAN_FD_CAN;//FDCAN_CLASSIC_CAN;
TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
TxHeader.MessageMarker = 0;
HAL_DAC_Start(&hdac1, DAC1_CHANNEL_1);
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1, 20);
HAL_I2C_EnableListen_IT(&hi2c4);
/* USER CODE END 2 */
/* Init scheduler */
osKernelInitialize();
/* Call init function for freertos objects (in freertos.c) */
MX_FREERTOS_Init();
LamikTask_Init();
LamikQueue_Init();
LEDTask_Init();
LEDQueue_Init();
EGTLTask_Init();
EGTLQueue_Init();
EGTRTask_Init();
EGTRQueue_Init();
/* Start scheduler */
osKernelStart();
/* We should never get here as control is now taken by the scheduler */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
void FreeRTOSLoop()
{
temp_int = Max31855_Read_Temp(TempL_GPIO_Port,TempL_Pin) ;
SendToEGTL(temp_int,ErrorMax31855);
temp_int = Max31855_Read_Temp(TempR_GPIO_Port,TempR_Pin) ;
SendToEGTR(temp_int,ErrorMax31855);
TxData[0] = 0x10;
TxData[1] = 0x20;
TxData[2] = 0x30;
TxData[3] = 0x40;
TxData[4] = 0x50;
TxData[5] = 0x60;
TxData[6] = 0x70;
TxData[7] = 0x80;
if (HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, TxData) != HAL_OK)
{
Error_Handler();
}
strcpy(DisplayLCD,"send");
SendToLamik(DisplayLCD);
osDelay(500);
strcpy(DisplayLCD,"stop");
SendToLamik(DisplayLCD);
osDelay(500);
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
__HAL_RCC_SYSCFG_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_LSI
|RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
RCC_OscInitStruct.LSIState = RCC_LSI_ON;
RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 4;
RCC_OscInitStruct.PLL.PLLN = 240;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 24;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_2;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
{
Error_Handler();
}
HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_PLL1QCLK, RCC_MCODIV_1);
}
/**
* @brief Peripherals Common Clock Configuration
* @retval None
*/
void PeriphCommonClock_Config(void)
{
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/** Initializes the peripherals clock
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_ADC|RCC_PERIPHCLK_LTDC;
PeriphClkInitStruct.PLL3.PLL3M = 10;
PeriphClkInitStruct.PLL3.PLL3N = 181;
PeriphClkInitStruct.PLL3.PLL3P = 2;
PeriphClkInitStruct.PLL3.PLL3Q = 2;
PeriphClkInitStruct.PLL3.PLL3R = 4;
PeriphClkInitStruct.PLL3.PLL3RGE = RCC_PLL3VCIRANGE_0;
PeriphClkInitStruct.PLL3.PLL3VCOSEL = RCC_PLL3VCOWIDE;
PeriphClkInitStruct.PLL3.PLL3FRACN = 0;
PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_PLL3;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
}
I cant send or recived data. When canfilterconfig.FilterID1 = 0x100; and i send data from secound board riverdi lcd frozen and i can only reset board. But when i change to other ID like 0x101 no frozen. Callback Can is never performed