fdcan on Riverdi STM32H7 Embedded Display 7"
Hello,
I've started to develop with the Riverdi STM32 Embedded Display and I'm trying to use the CAN BUS to display data, but unfortunately I can't. I'm not receiving any data. The CAN on the board is a FDCAN and I've set it to classic, because that's the function I need to use. I'm not receiving any data. The baud rate is set to 500kbit/s as I need it, but whatever I send to the board via the CAN BUS, I'm not receiving it. I need to receive from any CAN BUS ID. I'm also trying to find information on how to send data properly between the Main -> model. I've found some information but it's 2-3 years old and I could use a little more help.
Thanks a lot.