FDCAN on STM32C0: transmitting every 100ms, receiver sees frames only every ~497ms
- December 10, 2025
- 6 replies
- 295 views
Post edited by ST moderator to be inline with the community rules for the code sharing. In next time please use </> button to paste your code and a linker script content. Please read this post: How to insert source code.
i, I am using STM32C092CCT6 with FDCAN.
I transmit one CAN frame every 100 ms (even tried 50 ms).
But on the receiver side, I always receive frames only every ~497 ms.
It looks like something is delaying or buffering the frames.
What I want to know:
Which FDCAN settings could cause the frames to appear only every ~497 ms?
My problem summary:
Tx interval configured: 100 ms → Rx sees ~497 ms
Tx interval configured: 50 ms → Rx still ~497 ms
So the transmit timing is not coming out correctly.
Request:
Please check if anything is wrong with my FDCAN configuration (below).
/**
* @brief FDCAN1 Initialization Function
* None
* @retval None
*/
static void MX_FDCAN1_Init(void)
{
/* USER CODE BEGIN FDCAN1_Init 0 */
/* USER CODE END FDCAN1_Init 0 */
/* USER CODE BEGIN FDCAN1_Init 1 */
/* USER CODE END FDCAN1_Init 1 */
hfdcan1.Instance = FDCAN1;
hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV1;
hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan1.Init.AutoRetransmission = DISABLE;
hfdcan1.Init.TransmitPause = DISABLE;
hfdcan1.Init.ProtocolException = DISABLE;
hfdcan1.Init.NominalPrescaler = 16;
hfdcan1.Init.NominalSyncJumpWidth = 1;
hfdcan1.Init.NominalTimeSeg1 = 58;
hfdcan1.Init.NominalTimeSeg2 = 1;
hfdcan1.Init.DataPrescaler = 1;
hfdcan1.Init.DataSyncJumpWidth = 1;
hfdcan1.Init.DataTimeSeg1 = 1;
hfdcan1.Init.DataTimeSeg2 = 1;
hfdcan1.Init.StdFiltersNbr = 0;
hfdcan1.Init.ExtFiltersNbr = 0;
hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN FDCAN1_Init 2 */
/* USER CODE END FDCAN1_Init 2 */
}