Flash erase blocking GPIO updates
I am testing doing flash erase while running code from internal SRAM on a STM32F072B Discovery Board. Having initializing everything with code running in flash, I call a function where itself and all its dependencies exist in RAM. I've verified this in many ways: code analysis, stepping through debugger, etc. I have also copied the ISR vectors to RAM at 0x2000_0000 and used SYSCFG_CFGR1 register to remap SRAM to 0x0000_0000.
I have TIM2_CH1 setup as a 100kHz timer and increment a tick variable each interrupt. The interrupt also toggles a GPIO pin every pulse. Currently that is connected to an LED so I can visualize what's going on, but I have tested with a bare pin at GPIO_SPEED_FREQ_HIGH as well with the same results.
All of this works fine as long as I don't do the flash erase cycle. But as soon as I erase a few pages of flash, the LED starts flickering quite a bit like the GPIO bus is being blocked. The datasheet says that flash should only block the flash bus; running in SRAM is supposed to avoid CPU stalls. The GPIO also doesn't seem to be on the same bus. So my question is why is this happening? I have attached some logic analyzer captures of the GPIO. In the macro view you can see two white blocks on the left and right ends. This is the 100kHz signal. Once the signal becomes sparse that is when flash erase is in progress. The toggling is extremely slow and erratic during this time frame. I also attached a close up on the 200kHz signal to show that it is functioning fine outside of the flash erase cycle.
I've also attached the project which is based off one of the examples in the SDK. I copied many functions into My_XXX variants to place them into RAM.