FMC SDRAM common clock description mismatch between CubeIDE and RM0433
I want to set up 100MHz for SDRAM.
STM32CubeIDE version 1.18.1 has the following options for SDRAM clock:

The selected board is the STM32H743IITx.
RM0433 Rev 8 states that:

I'm not sure HCLK and fmc_ker_ck are the same thing.
If I have my FMC clock set up as:

And select HCLK/2, I'll have 100MHz for the SDRAM? Or is HCKL system clock?