From H7-series to U5-series - problem with OCTOSPI
Hi,
I have two custom boards using the same OCTOSPI HyperFlash and for some reason the memory fails to run at higher speeds with U5-board.
Board 1
-H7 MCU at 550 MHz
-OCTOSPI at 160 MHz works fine! (max clk is 166 MHz)
Board 2
-H5 MCU at 160 MHz
-OCTOSPI at 160 MHz fails in W/R.... (works fine up to 110 MHz)
Could there be any specific reasons why the U5 cannot handle the OCTOSPI running at 160 MHz, which in this case is the same speed as the MCU clock?