Function to simulature quadratures changes quadrature direction randomly.
Hi,
I have these two functions ( see below ) that simulate, respectively, a positive and negative quadrature.
void TIM3_Configuration_positive_quadrature(void)
{
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
int Period;
Period = 1000 / 1; //
TIM_Cmd( TIM3, DISABLE );
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_TimeBaseStructure.TIM_Period = 1000 - 1;
//the prescaler is divided by 2 because the toggle mode (see below) halves the frequency.
TIM_TimeBaseStructure.TIM_Prescaler = ( TIM3_FREQ / lastSetFrequency ) / 2 - 1;
TIM_TimeBaseInit( TIM3, &TIM_TimeBaseStructure );
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OCInitStructure.TIM_Pulse = (Period * 1) / 4; // CH3 at 25%
TIM_OC3Init(TIM3, &TIM_OCInitStructure);
TIM_OC3PreloadConfig( TIM3, TIM_OCPreload_Enable );
TIM_OCInitStructure.TIM_Pulse = (Period * 3) / 4; // CH4 at 75%, ie half cycle later
TIM_OC4Init(TIM3, &TIM_OCInitStructure);
TIM_OC4PreloadConfig( TIM3, TIM_OCPreload_Enable );
TIM_Cmd( TIM3, ENABLE );
}
void TIM3_Configuration_negative_quadrature(void)
{
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
int Period;
Period = 1000 / 1;
TIM_Cmd( TIM3, DISABLE );
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_TimeBaseStructure.TIM_Period = 1000 - 1;
//the prescaler is divided by 2 because the toggle mode (see below) halves the frequency.
TIM_TimeBaseStructure.TIM_Prescaler = ( 84000 / lastSetFrequency ) / 2 - 1;
TIM_TimeBaseInit( TIM3, &TIM_TimeBaseStructure );
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OCInitStructure.TIM_Pulse = (Period * 3) / 4; // CH3 at 75%
TIM_OC3Init(TIM3, &TIM_OCInitStructure);
TIM_OCInitStructure.TIM_Pulse = (Period * 1) / 4; // CH4 at 25%, ie half cycle later
TIM_OC4Init(TIM3, &TIM_OCInitStructure);
TIM_Cmd( TIM3, ENABLE );
}
The first time I set the frequency and call the positive quadrature function I get the wanted phase shift; but when I call the function to set the frequency and call the positive quadrature function once again I get negative phase shifting, if I call the negative quadrature function I get positive quadrature instead; so they basically switch.
I've checked that the negative quadrature function doesn't get called.
Edit: If I change Frequency, only once, and call the positive quadrature twice i get positive and then negative quadrature.
Is there any workaround?