Skip to main content
Explorer II
February 27, 2025
Question

FW flashing from Bootloader

  • February 27, 2025
  • 1 reply
  • 1910 views

Hi , I am now working on FW upgrade using uart . Bootloader receives the application hex file through uart and flashes it .Then jumps to application , but facing some issues with flashing , flashing is not taking place. 

I am using NUCLEO-H723ZG board . I will attach the zip file of the project . 

    This topic has been closed for replies.

    1 reply

    Graduate II
    February 27, 2025

    Do you have any error to share? any trace? any log?

    CJ007Author
    Explorer II
    February 27, 2025

    CJ007_0-1740645460774.png

    Hi @urbito what do you mean? I only have these debug prints from docklight.After the flashing , no data is found at Application start address area, thus not jumping to application. I have a doubt whether is it because of the approach i took. Thats why I shared the zip file of the project I worked.

    Explorer
    February 27, 2025

    > After the flashing , no data is found at Application start address area, ...

    Obviously, your flashing does not work.
    Do you verify each address ?

    Or try to read out the flash after an update by the bootloader.
    If this shows the same result, you need to work on your flash routine.