G474 clarification about RM0440 "3.3.5 Flash program and erase operations"
I have developed a program that performs IAP (In-Application Programming). I am using single bank mode.
The manual states:
"An on-going Flash memory operation does not block the CPU as long as the CPU does not access the same Flash memory bank."
However, I didn't notice any problem.
My program runs in the address range 0x8000000-0x8010000 and the IAP programs the higher addresses.
If the CPU is blocked what happen? If my program can wait I have to care just about watchdog?
Thank you
Best Regards
Marco