Get witch line has called Error_Handler(void)
Hi, I'm trying to develop a FW for one of my custom boards that has an ethernet interface.
I'm using STM32CubeIDE, I generated the code with the configurator, and without even writing a line of code, if I go into debug, during the initialization of the HAL the code immediately jumps to:
void Error_Handler(void){
I wanted to ask, Is there a way to know at which point the code jumped to Error_Handler(void), so as to try to understand where the problem is.
In other words, is it possible to run the code backwards or see from which line a certain function was called?