Getting Started with CAN Communication on Nucleo F446RE


Hello STM32 Community,
I'm trying to implement CAN communication on my Nucleo F446RE board and I'm facing some challenges getting it to work properly. I've attached screenshots of my .ioc configuration and the auto-generated code from STM32CubeIDE for reference.
Current Setup
Hardware: STM32 Nucleo F446RE
Transceiver: SN65HVD230
Baudrate: 500kbps (Prescaler=5, BS1=6TQ, BS2=3TQ)
IDE: STM32CubeIDE
Issues I'm Experiencing
When trying to transmit CAN messages, I'm getting "TX Error" and "CAN State: RESET" messages through UART. The free TX mailboxes show as 0, which seems unusual for initialisation.
What I've Tried
Configured CAN1 in normal mode
Set up the pins PA11 (RX) and PA12 (TX) for CAN
Implemented basic transmission code using HAL_CAN_AddTxMessage()
Added proper termination resistors (120Ω)
Questions
Is my CAN configuration correct in the .ioc file?
What could be causing the CAN peripheral to remain in RESET state?
Are there any specific initialization steps I'm missing for the SN65HVD230 transceiver?
How can I properly verify if my hardware connections are correct?
I'm planning to communicate with another STM32 board (L432KC) using CAN, but I need to get the basic transmission working first.
Any help, examples, or guidance would be greatly appreciated!
Thank you in advance,
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2025 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
CAN_HandleTypeDef hcan1;
UART_HandleTypeDef huart2;
/* USER CODE BEGIN PV */
CAN_TxHeaderTypeDef TxHeader;
uint8_t TxData[8];
uint32_t TxMailbox;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_CAN1_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
void HAL_GPIO_EXITI_Callback(uint16_t GPIO_Pin)
{
if (GPIO_Pin == GPIO_PIN_13){
TxData[0] = 100; // ms Delay
TxData[1] = 10; // loop rep
HAL_CAN_AddTxMessage(&hcan1, &TxHeader, TxData, &TxMailbox);
}
}
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
char msg[50]; // Buffer for debug messages
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_CAN1_Init();
/* USER CODE BEGIN 2 */
// Send an initial debug message to confirm USART2 is working
sprintf(msg, "USART2 working!\r\n");
HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), 1000);
HAL_CAN_Start(&hcan1);
//Activate the notification
HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING);
TxHeader.DLC = 2; // data length
TxHeader.IDE = CAN_ID_STD;
TxHeader.RTR = CAN_RTR_DATA;
TxHeader.StdId = 0x446; // ID
TxData[0] = 50;
TxData[1] = 0xAA;
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1) {
// Prepare data
static uint8_t counter = 0;
TxData[0] = 'A' + (counter++ % 26); // Cycle through A-Z
// Send CAN message
if (HAL_CAN_AddTxMessage(&hcan1, &TxHeader, TxData, &TxMailbox) != HAL_OK) {
char err_msg[] = "TX Error\r\n";
HAL_UART_Transmit(&huart2, (uint8_t*)err_msg, strlen(err_msg), 100);
}
else {
char debug_msg[50];
sprintf(debug_msg, "Sent: %c (ID: 0x%03lX)\r\n", TxData[0], TxHeader.StdId);
HAL_UART_Transmit(&huart2, (uint8_t*)debug_msg, strlen(debug_msg), 100);
}
CheckCANStatus();
HAL_Delay(2000); // 1Hz transmission
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
/* USER CODE END 3 */
}
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 16;
RCC_OscInitStruct.PLL.PLLN = 200;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief CAN1 Initialization Function
* None
* @retval None
*/
static void MX_CAN1_Init(void)
{
/* USER CODE BEGIN CAN1_Init 0 */
/* USER CODE END CAN1_Init 0 */
/* USER CODE BEGIN CAN1_Init 1 */
/* USER CODE END CAN1_Init 1 */
hcan1.Instance = CAN1;
hcan1.Init.Prescaler = 5;
hcan1.Init.Mode = CAN_MODE_NORMAL;
hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan1.Init.TimeSeg1 = CAN_BS1_6TQ;
hcan1.Init.TimeSeg2 = CAN_BS2_3TQ;
hcan1.Init.TimeTriggeredMode = DISABLE;
hcan1.Init.AutoBusOff = DISABLE;
hcan1.Init.AutoWakeUp = DISABLE;
hcan1.Init.AutoRetransmission = DISABLE;
hcan1.Init.ReceiveFifoLocked = DISABLE;
hcan1.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN1_Init 2 */
/* USER CODE END CAN1_Init 2 */
}
/**
* @brief USART2 Initialization Function
* None
* @retval None
*/
static void MX_USART2_UART_Init(void)
{
/* USER CODE BEGIN USART2_Init 0 */
/* USER CODE END USART2_Init 0 */
/* USER CODE BEGIN USART2_Init 1 */
/* USER CODE END USART2_Init 1 */
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */
/* USER CODE END USART2_Init 2 */
}
/**
* @brief GPIO Initialization Function
* None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin : B1_Pin */
GPIO_InitStruct.Pin = B1_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pin : LD2_Pin */
GPIO_InitStruct.Pin = LD2_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(LD2_GPIO_Port, &GPIO_InitStruct);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
void CheckCANStatus(CAN_HandleTypeDef *hcan) {
// Get current state
HAL_CAN_StateTypeDef state = HAL_CAN_GetState(hcan);
uint32_t errorCode = HAL_CAN_GetError(hcan);
char statusMsg[100];
// Report state
switch(state) {
case HAL_CAN_STATE_RESET:
sprintf(statusMsg, "CAN State: RESET\r\n");
break;
case HAL_CAN_STATE_READY:
sprintf(statusMsg, "CAN State: READY\r\n");
break;
case HAL_CAN_STATE_LISTENING:
sprintf(statusMsg, "CAN State: LISTENING\r\n");
break;
case HAL_CAN_STATE_SLEEP_PENDING:
sprintf(statusMsg, "CAN State: SLEEP PENDING\r\n");
break;
case HAL_CAN_STATE_SLEEP_ACTIVE:
sprintf(statusMsg, "CAN State: SLEEP ACTIVE\r\n");
break;
case HAL_CAN_STATE_ERROR:
sprintf(statusMsg, "CAN State: ERROR\r\n");
break;
default:
sprintf(statusMsg, "CAN State: UNKNOWN\r\n");
}
HAL_UART_Transmit(&huart2, (uint8_t*)statusMsg, strlen(statusMsg), 100);
// Report any errors
if (errorCode != HAL_CAN_ERROR_NONE) {
if (errorCode & HAL_CAN_ERROR_EWG)
HAL_UART_Transmit(&huart2, (uint8_t*)"Error: Warning\r\n", 16, 100);
if (errorCode & HAL_CAN_ERROR_EPV)
HAL_UART_Transmit(&huart2, (uint8_t*)"Error: Passive\r\n", 16, 100);
if (errorCode & HAL_CAN_ERROR_BOF)
HAL_UART_Transmit(&huart2, (uint8_t*)"Error: Bus-off\r\n", 16, 100);
if (errorCode & HAL_CAN_ERROR_ACK)
HAL_UART_Transmit(&huart2, (uint8_t*)"Error: No ACK\r\n", 15, 100);
// Reset errors after reporting
HAL_CAN_ResetError(hcan);
}
// Report TX status
uint32_t txFree = HAL_CAN_GetTxMailboxesFreeLevel(hcan);
sprintf(statusMsg, "Free TX mailboxes: %lu\r\n", txFree);
HAL_UART_Transmit(&huart2, (uint8_t*)statusMsg, strlen(statusMsg), 100);
}
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* file: pointer to the source file name
* line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */