GPIO going to zero in STOP3 Mode even if connected with internal pull-up STM32U5A5
Hello,
I'm developing an application on the NUCLEO-U5A5ZJ-Q. I need some pins to stay high while the microcontroller is in Stop3 mode.
The Datasheet suggests to use internal pull ups, because the GPIO peripheral is not active in Stop3 mode. For this reason, I have configured the GPIO as input and with internal pull-up before entering Stop3 mode.
I've used the following functions:
LL_GPIO_SetPinPull(GPIOC, LL_GPIO_PIN_6, GPIO_PULLUP);
LL_GPIO_SetPinMode(GPIOC, LL_GPIO_PIN_6, LL_GPIO_MODE_INPUT);
It works and the pin stays high. However, whenever the microcontroller go into Stop3 mode, the GPIO voltage goes to zero.
Any Idea? Am I missing something?
Thank you in Advance