GPIO Latency STM32F411 Blackpill
Hello All,
I am doing this post after trying everything I can to solve my Issue.
I have a STM32F411 Blackpill connected on an Apple II Bus Slot.
The Apple II has a clock (Phi0) close to 1 Mhz. Phi0 is connected to Pin A2 where I have setup a Falling & Rising Edge interrupt.
The GPIO B12 is used to check the latency between each Phi0 phase,
- at the falling edge of Phi0 B13 is clear
- at the rising edge of Phi0 B13 is set,
I have nothing else running on this STM32, I am observing a delay (avg 335 ns) between the interrupt detection and GPIO set or clear.
Using the logic analyzer:

Debug2 is the GPIO B13
I use the following code :
#define GPIO_SET_PIN(port, pin) ((port)->BSRR = (pin))
#define GPIO_CLEAR_PIN(port, pin) ((port)->BSRR = (pin << 16u))
#pragma GCC push_options
#pragma GCC optimize ("-Ofast")
void EXTI2_IRQHandler(void){
__HAL_GPIO_EXTI_CLEAR_IT(PHI0_Pin);
if ((PHI0_GPIO_Port->IDR & PHI0_Pin)==0){
GPIO_CLEAR_PIN(DEBUG1_GPIO_Port,DEBUG1_Pin);
}else{
GPIO_SET_PIN(DEBUG1_GPIO_Port,DEBUG1_Pin);
}
}
#pragma GCC pop_optionsThe clock setting :
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 25;
RCC_OscInitStruct.PLL.PLLN = 384;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
RCC_OscInitStruct.PLL.PLLQ = 8;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
Error_Handler();
}
}The GPIO Settings:
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_13, GPIO_PIN_RESET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOA, D_CE_Pin|D_DIR_Pin|IRQ_DRV_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOB, DEBUG1_Pin|DEBUG2_Pin|A_CE1_Pin|A_CE2_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin : PC13 */
GPIO_InitStruct.Pin = GPIO_PIN_13;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/*Configure GPIO pins : RW_Pin DEVSEL_Pin */
GPIO_InitStruct.Pin = RW_Pin|DEVSEL_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pin : PHI0_Pin */
GPIO_InitStruct.Pin = PHI0_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING_FALLING;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(PHI0_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pins : D_CE_Pin D_DIR_Pin IRQ_DRV_Pin */
GPIO_InitStruct.Pin = D_CE_Pin|D_DIR_Pin|IRQ_DRV_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pins : SD_EJECT_Pin RESET_Pin */
GPIO_InitStruct.Pin = SD_EJECT_Pin|RESET_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pins : DA0_Pin DA1_Pin DA2_Pin DA3_Pin
DA4_Pin DA5_Pin DA6_Pin DA7_Pin */
GPIO_InitStruct.Pin = DA0_Pin|DA1_Pin|DA2_Pin|DA3_Pin
|DA4_Pin|DA5_Pin|DA6_Pin|DA7_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/*Configure GPIO pins : DEBUG1_Pin DEBUG2_Pin */
GPIO_InitStruct.Pin = DEBUG1_Pin|DEBUG2_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/*Configure GPIO pins : A_CE1_Pin A_CE2_Pin */
GPIO_InitStruct.Pin = A_CE1_Pin|A_CE2_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* EXTI interrupt init*/
HAL_NVIC_SetPriority(EXTI2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI2_IRQn);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}Why do I have a huge latency between B13 & PHI0 ?
What can I change / do to reduce that gap ?
Thank
Vincent