GPIO output pulse stability (bis)
Hello,
Trying to do precise GPIO pulses with assembly code - on any STM Nucleo board - shows jitter and fluctuating frequency. I was told by a super user to do it via PWM
I would like to add some comment that may be interesting for others :
- trying to do precise pulses with PWM on the Nucleo H723 for example, still shows jitter and fluctuating frequency around the desire value. Same using HSE or HSI. Same with Nucleo-F411. Same with Nucleo-N667. I understand the reasons now.
But playing around the Nucleo-N657, I got some success : if you feed your CPU_clock directly with HSE (48MHz on board), and feed the other peripherals, including timer_clock with HSE+PLL (400MHz for example), then the resulting PWM is quite accurate and stable !
Regards,