GPIO Read interact with GND or VCC
Hi,
I use STM32F103C8T6 a GPIO input pin to read a high or low signal from another GPIO output pin, and connect a 3Mohm resistor between two pins, and I notice touching GND with hand will influence the signal status, than I measure the resistance between GND and GPIO pin, it is around 10Mohm. I want to isolate the signal from GND interference, how should I do? I have to keep 3 Mohm resistor. will it be better if connect a capacitor between input pin and GND? or connect a large resistor in between?