Skip to main content
Explorer II
October 14, 2024
Solved

GPIO Trouble on STM32 F767ZI

  • October 14, 2024
  • 8 replies
  • 4283 views

I used a Nucleo F767ZI dev board to check and write firmware
(The IC on the board is STM32F767ZIT6U with the other characters being AA 254 VQ Z on first line and TWN AA 341 on line 2),
when I use HSI clock I am able to operate PD7, PG9, PG10, PG11, PG12 as an input or output GPIO
But on the custom developed board (the IC on the board is STM32F767ZIT6 with the other characters being AA108 VQ on the first line and TWN AA 334 on line two)

In this custom developed board while I am able to Program and debug the board and I am able to use all other pins except PD7, PG9, PG10, PG11, PG121)

1)The DC resistance of each of the above mentioned Pin and VCC(3V3) is infinite and same is with GND is also infinite

2) When I configure any of these Pins as GPIO Output as PUSH PULL and low speed mode then I see when I set the GPIO I see as the ODR setting but when I measure the voltage on the connecter(nothing between the connecter and the MCU Pin and tack length is less than 5 cms) i see 0.5 to 0.6V
3) When I configure any of these pins as Input with no Internal Pull or Pull Down, I see that these pins are not affected by noise where as other working pins are and if I connected 3V3 from a jumper cable to read input as logic High even that fails other than these 5 pins all other pins are working as expected.

Please help to debug the issue.

    This topic has been closed for replies.
    Best answer by Chris21

    This seems very likely to be involved:

    "The VDDSDMMC is an independent power supply for SDMMC2 peripheral IOs (PD6, PD7,
    PG9..12). It can be connected either to V DD or an external independent power supply."

    Chris21_0-1729018282476.png

     

    8 replies

    Super User
    October 14, 2024

    @akash_praan wrote:

    In this custom developed board


    Please provide the schematics for this board.

     

    Explorer II
    October 15, 2024

    Hi @Andrew Neil , please find the schematic 

    akash_praan_1-1728970300622.png

    akash_praan_2-1728970347530.png

     

    I am able to Program the board, 

    GPIO Clock are defined (generated by Cube MX) properly, I am able to use all pins other than the 5 mentioned above. 
    There is no extra component between the Pins and the connector and the length of each trace is also less than 6 to 7 cms. There is proper connectivity between the MCU pins and the connector Pads and Infinite DC Resistance between the MCU Pins and VCC, also between MCU Pins and GND

    Surprisingly all 5 pins that don't work are connected between C28 and C6

    akash_praan_0-1728970928764.png

     

     

    Explorer II
    October 15, 2024

    @Andrew Neil  Thank you for your time on this problem, if you need anything else to have a better understanding, please let me know. 

    Super User
    October 15, 2024

    That's not a schematic - it doesn't show what is actually connected to the processor pins

    Explorer II
    October 15, 2024

    @Andrew Neil Please find the required schematic parts for complete reference

    . There is nothing between the MCU pin and the connector 

    akash_praan_0-1729064259689.png

     

    akash_praan_3-1729064316782.png

     

    akash_praan_5-1729064364983.png

     

     

     

     

     

     

    Graduate II
    October 15, 2024

    So all these 5 pins are connected directly to the connector.

    1) Have you removed the connector and then tested the GPIOs ?

    2) Maybe the board / connector had some ESD stress? Was it assembled / used in an ESD-safe environment?

    3) Do you have another board to check?

    Graduate
    October 15, 2024

    You need provide 1.8 v or 3.3v to vddsdmmc pin 132?

    Graduate
    October 15, 2024

    Pin 121

    Explorer II
    October 15, 2024

    https://www.st.com/en/microcontrollers-microprocessors/stm32f767zi.html
    @Richard Li 
    According to datasheet section 3.17, as per my understanding that needs to be done only when SDMMC i being used, but I will try connecting to 3.3V and then try it as all the mentioned pins which are not working have SDMMC as Alternate functions available. 

    Thank you for you suggestion. 

    @all please help me if my understanding is incorrect.

    Explorer II
    October 15, 2024

    Sure, I will try this out in the office in another 10 hours and see what the result. Most likely this should be it. 

    Thank you for pointing this out. 

    Regards,
    Akash Rao

    Graduate
    October 15, 2024

    Beside the VDDSDMMC float, I don't understand why measure resistance for GND is like floating, You may need check pin 130 GND.

    Graduate
    October 15, 2024

    Another interesting observation.  Schematic only shows one VSS pin connected, ther should be 10.

    Explorer II
    October 16, 2024

    After the VDDSDMMC being connected, all pins work as intended. This was the error

    VSS is internally connected as I verified in the Layout as well as the Hardware. 

    Thank you for your help @Chris21 @Andrew Neil @LCE @Richard Li 

    Graduate
    October 16, 2024

    Not sure what you mean by: "VSS is internally connected".

    ST's guidance:

    All the power supply and ground pins must be properly connected to the power supplies.
    These connections, including pads, tracks and vias should have as low impedance as
    possible. This is typically achieved with thick track widths and, preferably, the use of
    dedicated power supply planes in multilayer PCBs.


    In addition, each power supply pair should be decoupled with filtering ceramic capacitors
    (100 nF) and one single tantalum or ceramic capacitor (min. 4.7 μF) connected in parallel.
    These capacitors need to be placed as close as possible to, or below, the appropriate pins
    on the underside of the PCB. Typical values are 10 nF to 100 nF, but the exact values
    depend on the application needs. Figure 23 shows the typical layout of such a VDD/VSS pair.

    Graduate II
    October 16, 2024

    Not sure what you mean by: "VSS is internally connected".

    The PCB layout screenshot shows that the GND pins are connected to GND underneath the package.

    And some CAD apps' schematic symbols do not show all VCC or GND pins. I hate that, and rather draw my own...