Skip to main content
Graduate
January 29, 2024
Question

H5 and FREERTOS

  • January 29, 2024
  • 1 reply
  • 2498 views

Hi to everybody.

 

I've developed an application using FreeRTOS, under M3 Series.

Then moved to M4 without probelms. In CubeMX I can add all the tasks, timers, Mutex and so on.

2024-01-29_12h47_04.png

Now I'm porting to H5 MCU, but the freertos disappear from CubeMX. I found the X-CUBE-FREERTOS, where I must select "something" as this:

TheRaprus_0-1706529121406.png

I really donnow why Heap_4 (not 3 or 5), and that is TZ_Not Supported.

But now? How I can I reuse my old source w/o revrite everythig?

Is what I did correct? Why H5 is different between M3/M4?

Thanks!

 

    This topic has been closed for replies.

    1 reply

    ST Employee
    January 29, 2024

    Hello @TheRaprus

    X-CUBE-FREERTOS provides a full integration of the FreeRTOS kernel in the STM32Cube environment for the STM32H5 series, STM32C0 series, STM32U5 series, and STM32WBA series (newer series, not related to Cortex) 

    You can download X-Cube-FREERTOS, and you can find examples with configured .ioc files