H5 DMA - How to start
I'm trying to implement a SPI transfer between flash and SPI2 - a simple display. I'm using LL everywhere.
No problem with M3 and M4 - But GPDMA is completely different. "Normal" SPI work but no way to enable DMA.
Based on the only example with LL (All the examples are flash to ram only!). I wrote this:
LL_DMA_SetSrcAddress(GPDMA1, LL_DMA_CHANNEL_0, (uint32_t)&icon1);
LL_DMA_SetDestAddress(GPDMA1, LL_DMA_CHANNEL_0, LL_SPI_DMA_GetTxRegAddr(SPI2));
LL_DMA_SetBlkDataLength(GPDMA1, LL_DMA_CHANNEL_0, icon1_size_byte);
/* Enable DMA transfer complete/error interrupts */
LL_DMA_EnableIT_TC(GPDMA1, LL_DMA_CHANNEL_0);
LL_DMA_EnableIT_DTE(GPDMA1, LL_DMA_CHANNEL_0);
/* Start the DMA transfer Flash to Memory */
LL_DMA_EnableChannel(GPDMA1, LL_DMA_CHANNEL_0);Icon size is about 2kB. Unfortunately no interrupt occours.
I'll hope that some example will be added on the next H5 update (HAL &LL).
Any suggestions?