H743VI - pin dies away -- reliability problem of chip ?
Hi,
Just yesterday on my H743VIT6 (rev. V ) on the running TFT : picture faded away...white screen.
I just happened to look at the display , thinking ...ok, maybe one of the thin wires just broke now...
TFT (small, 1,8" , ST7735 on 3,3V) connected /soldered about May 2022 , on SPI2 , at 48 Mbit . :)
(Not touched/changed the wiring since then - so no static problem etc. possible.)
Today i tried to fix the problem - but everything still connected !
So took the scope to check the signals, beginning with reset ...all look ok, except SPI data !
Here super slow rise time...ok, no useful signal for the TFT at 48Mb. (PC3_3 is sick ?)
First check short to next pins - no, all free. Then impedance of pin unpowered : high, as cmos should be.
Hmmm....try other pin: in Cube could choose PC1 as SPI2 data tx , so i changed to this and soldered the wire also here. (Soldering iron is antistatic.)
Hey, TFT display ok, as before.
But was the pin the problem - after 1 1/2 years running ?? So i set it as gpio out , hi speed, and put simple gpio toggle to it, this its doing now (looks like heavy capactive loaded - but just the 20pF of scope probe there):

Seems this pin lost its drive power all by itself !
Now the crucial question : first sign of dying chip ? or why can this happen ?
(I never seen something like this on any cpu , by STM or others.)
And cpu just at 200MHz core clk, (for longer life...), about 30,3° C case (IR therm.).