HAL_CAN_AddTxMessage() contains problems
Hi
I am using CAN in STM32F303RDT6.
I am using HAL_CAN_AddTxMessage for CAN transmission.
This function will send the data and return HAL_OK if the sending mailbox is free.
However, although HAL_CAN_AddTxMessage returns HAL_OK, no message may actually be output on the CAN bus.
I am using CANoe to monitor a CAN bus.
My application has a queue that stores outgoing messages that I create. The application writes outgoing data to the queue at any time.
The data retrieved from the queue is input to HAL_CAN_AddTxMessage. When HAL_OK is returned, it is assumed that the data has been sent and the next queue data is retrieved.
However, even though HAL_OK is returned, there are times when it is not output to the CAN bus. This is a problem.
Please tell me any countermeasures.
Help Me.....