HAL_I2C_Master_Transmit works, HAL_I2C_Master_Transmit_IT does not.
I’m trying to replace a blocking call to HAL_I2C_Master_Transmit() with the interrupt version HAL_I2C_Master_Transmit_IT(). The blocking HAL_I2C_Master_Transmit() call works perfectly. The HAL_I2C_Master_Transmit_IT() call sends completely different data. Specifically:
My buffer contains: 00 00 00 00 00 00 00 BF 00 3F 00 00 00 00 00 00 00
When I call HAL_I2C_Master_Transmit(&hi2c4, I2C_ADDRESS, buffer, 17, 100), I see this:

When I call HAL_I2C_Master_Transmit_IT(&hi2c4, I2C_ADDRESS, buffer, 17), I see unrecognized data:

I’m using a STM32H755.