Has anyone else struggled with the MX3080/M1400 Wi‑Fi modules?
Honestly, this choice feels like a trap.
STM keeps promoting it as a “solution,” but compared to Murata, ESP32, or Broadcom it looks outdated:
– Legacy M4 core, original MXCHIP code from 2017
– Closed software, very little documentation
– Hard to debug (no sequence diagrams, no clear dedicated examples)
– Rare, unpolished firmware updates
– No Nucleo board for hands‑on exploration
– Doesn’t seem seriously supported by MXCHIP anymore (similar by STM)
This isn’t a shallow impression — I spent three weeks with console access and a logic analyzer writing and debugging code on the B‑U585I‑IOT2A board, and the friction was constant.
Curious if others see the same issues, or if there’s a hidden advantage I’m missing?