Having Problems activating SysTick after Stop mode
I'm using STM32F070CBT at 8mhz with almost all pins active (used for GPIOs, PWM, SPI,I2C,etc) , i'm using a timer to enter stop mode with low power regulator and waking up using GPIO external event, after waking up i checked that PWMs and GPIOs are still working but SysTick seems to have stopped as all delay functions enter a infinite loop on HAL_GetTick inside the delay function and SysTick_Handler is not being called anymore (i tested that using breakpoints) , i tried to activate SysTick again using :
- Hal_Init();
- HAL_ResumeTick();
- HAL_InitTick(0);
- SysTick->CTRL=0b011;
also tried to set SysTick priority to 0, also tried to recall "SystemClock_Config();" alongside SysTick activate function but it didn't work too , does anybody know what i need to do in order to re-activate SysTick?