Hello - a newbie looking for very basic documentation.
Hello world. This is my first post to the forum so please be tolerant if I inadvertently breach local etiquette.
I have some experience with RPi, Mbed and Arduino systems but none with the STM32F range until very recently when I was given a few kits to play with. Unfortunately absolutely no documentation was provided with any of them. The STM32F769I-EVAL will serve as an initial example, as that is the one with which I have been playing for a few hours. It powers up and displays lights, some of which flash under certain circumstances, and sometimes appears as a USB disk drive on the development computer. That drive contains precisely one file.
A vast range of documentation is available and I have downloaded a selection, along with development software. I am using a Ubuntu 23.10 amd64 system; The IDE fires up correctly, as far as I can tell. However, no documentation yet found is at a sufficiently basic level to enable me to make use of the material I do have. Neither have I yet found anything appropriate on YouTube.
What I need to know is along the lines of which of the four mini-B USB sockets to connect to the computer; which position the switch should be in; which jumpers must or must not be present; how the board appears to the computer and what additional software may be necessary for communicating; and so on.
Can anyone point me at the sort of documentation I need please?
Thanks,
Paul