Help Choosing the Right STM32 Chip for My VCU Project
Hi everyone,
I started designing PCBs last year and have completed a few projects using Arduino and ESP32. For my new project, however, I need to use an STM32 microcontroller. I could technically use an ESP32 as well, but STM32 is more suitable for industrial applications, so I decided to switch.
I already have a STM32F401CCU6 Black Pill board, and I can use that chip — but I’d like to ask for advice: Is there a better STM32 option for my project?
Here’s a brief description of the project:
I’m building a Vehicle Control Unit (VCU) for the Teknofest Efficiency Challenge Race. The race is mostly focused on minimizing power consumption.
In the VCU, I need to connect and manage the following components:
3 × DS18B20 temperature sensors
1 × Hall-effect or proximity sensor
1 × LoRa module
1 × SD card module
1 × Nextion HMI screen
1 × relay
Any suggestions or guidance about which STM32 chip would be most suitable are greatly appreciated.
Thanks a lot for your help!