Help with BlackPill STMF32411and Hex File for Absolute Musician Beginner for Midi Controller?
Hello!
I bought a BlackPill board, and need to upload ("flash"?) a hex-file to it.
It's for a simple musical midi controller.
I tried using Arduino once, and could copy the code to the Arduino IDE app, connect the RP Pico, and upload the code to the board, done!
I reconnect the Pico to my MacBook and the BlackPill is now a USB Midi controller.
They also have a file for the BlackPill STMF32411, in either .hex or .bin form.
I downloaded them both.
I'm on a MacBook running Big Sur.
The BlackPill has more ins and outs for switches, pots, etc., so I bought one.
Is there a simple way to upload this file to the BlackPill without allot of technical knowledge?
I should say without ANY technical knowledge?
I figured out the button sequence to put the BlackPill in bootloader mode, but the few things I tried didn't work, and frankly I don't have any idea what I am doing.
Just need to upload one of the two files to the BlackPill.
Any help would be much appreciated.
Thanks!!!