Help with STM32U0 RTC not running wanted
Hello,
probably I miss something, but I have searched long enough so things start to get unclear.
I have set up RTC on STM32U0, so I expect is to be running. But ist does not free running:
<(gdb) mon s
Target voltage: 3.24V
Available Targets:
No. Att Driver
1 STM32U07 M0+
(gdb) att 1
Attaching to program: /samsung/home/bon/devel/en_apps/caltime/stm32u083c-dk/caltime.elf, Remote target
0x08004a00 in Stm32RtcV2PollSync ()
at /samsung/home/bon/devel/en_apps/ethernut/nut/arch/cm3/dev/stm/stm32_rtc_v2.c:110
110 while ((RTC->ICSR & RTC_ICSR_RSF) != RTC_ICSR_RSF);
(gdb) p /x *RTC
$1 = {TR = 0x164928, DR = 0x249024, SSR = 0xff, ICSR = 0x17, PRER = 0x7f00ff, WUTR = 0xffff,
CR = 0x3000, RESERVED0 = {0x0, 0x0}, WPR = 0x0, CALR = 0x0, SHIFTR = 0x0, TSTR = 0x0,
TSDR = 0x0, TSSSR = 0x0, RESERVED1 = 0x0, ALRMAR = 0x0, ALRMASSR = 0x0, ALRMBR = 0x0,
ALRMBSSR = 0x0, SR = 0x0, MISR = 0x0, RESERVED2 = 0x0, SCR = 0x0, RESERVED3 = {0x0, 0x0, 0x0,
0x0}, ALRABINR = 0x0, ALRBBINR = 0x0}
(gdb) p /x *RTC
$2 = {TR = 0x164928, DR = 0x249024, SSR = 0xff, ICSR = 0x17, PRER = 0x7f00ff, WUTR = 0xffff,
CR = 0x3000, RESERVED0 = {0x0, 0x0}, WPR = 0x0, CALR = 0x0, SHIFTR = 0x0, TSTR = 0x0,
TSDR = 0x0, TSSSR = 0x0, RESERVED1 = 0x0, ALRMAR = 0x0, ALRMASSR = 0x0, ALRMBR = 0x0,
ALRMBSSR = 0x0, SR = 0x0, MISR = 0x0, RESERVED2 = 0x0, SCR = 0x0, RESERVED3 = {0x0, 0x0, 0x0,
0x0}, ALRABINR = 0x0, ALRBBINR = 0x0}
(gdb) p /x RCC->BDCR
$3 = 0x8103
(gdb) p /x RCC->APBSMENR1 & RCC_APBSMENR1_RTCAPBSMEN
$4 = 0x400
(gdb) p /x RCC->APBENR1 & RCC_APBENR1_RTCAPBEN
$5 = 0x400
(gdb) c
Continuing.
^C
Program received signal SIGINT, Interrupt.
Stm32RtcGetClock (rtc=0x2000040c <rtcStm32>, tm=0x20000c1c)
at /samsung/home/bon/devel/en_apps/ethernut/nut/arch/cm3/dev/stm/stm32_rtc_v2.c:356
356 Stm32RtcV2PollSync();
(gdb) p /x RCC->APBENR1 & RCC_APBENR1_RTCAPBEN
$6 = 0x400
(gdb) p /x *RTC
$7 = {TR = 0x164928, DR = 0x249024, SSR = 0xff, ICSR = 0x17, PRER = 0x7f00ff, WUTR = 0xffff,
CR = 0x3000, RESERVED0 = {0x0, 0x0}, WPR = 0x0, CALR = 0x0, SHIFTR = 0x0, TSTR = 0x0,
TSDR = 0x0, TSSSR = 0x0, RESERVED1 = 0x0, ALRMAR = 0x0, ALRMASSR = 0x0, ALRMBR = 0x0,
ALRMBSSR = 0x0, SR = 0x0, MISR = 0x0, RESERVED2 = 0x0, SCR = 0x0, RESERVED3 = {0x0, 0x0, 0x0,
0x0}, ALRABINR = 0x0, ALRBBINR = 0x0}>
This is on a stm32u583c-dk board. LSE is select and running. ABH clock enabled in normal and in sleep mode etc. RSF never gets set again and debugger also reads no new RTC values.
Any ideas? Thanks