How can I enable multiple clients to send queries to an Azure RTOS NetX TCP/IP server on an STM32H5
In my project, I have a TCP/IP server application running. My main problem is that only one client can connect to the same IP and port at the same time. My project requirement is that multiple clients should be able to send queries to the same IP and port. I can achieve this structure with LWIP, but I couldn't set up the same structure with Azure RTOS NetX. One client works without a problem, but multiple clients cannot send queries. What can we do about this?