How do I generate a Timer Interrupt at the completion of a series of pulses?
Using an Advanced Timer (Timer 1 in STM32H743ZI) in PWM One-Shot mode, and using the Repetition Counter, I generate a string of 5 pulses. For each pulse, I generate a Capture/Compare Interrupt and have a CallBack routine (using "HAL_TIM_PulseFinishedCallBack(...)". This works fine.
I have also enabled the Update Interrupt for Timer 1 and expected it to service that routine at the completion of the 5 pulses as well but it does not. The code for the Interrupt is generated in the stm32h7xx_it.c file "(void TIM1_UP_IRQHandler(void))" but execution does not appear to reach it. Both Timer 1 Capture/Compare and Update Interrupts are enabled in the NVIC. I am using "void HAL_TIM_Period_ElapsedCallback(...)" as the call back routine for the Update Interrupt.
How do I get the Update Interrupt to work?