How do I generate an Output Compare square wave on TIM8_CH2N using STM32CubeIDE?
I'm working with the STM32F407G-DISC1 development board and I would like to generate a square wave on PB14 (TIM8_CH2N). I'm able to successfully toggle PB14 using "bit-banging" and I'm able to successfully generate square waves PC6 (TIM8_CH1) and PC8 (TIM8_CH3). However, no matter what I do, I can't make TIM8 output anything on PB14 (TIM8_CH2N). Does anybody know what I'm doing wrong (please see attached screenshot)? Please note that I can't use any other timer/pin instead.