How do I set up DMA to circular mode on STM32H5 without HAL
Hello,
I am looking for a way to set up DMA to transfer from peripheral to circular buffer triggered from Timer
I hoped I could set it up just like it is described here, just change the source:
It samples data as expected but only once, it does not repeat when all 256 samples are taken.
Do I understand that picture wrong or is it bad? Do I need to do some more settings? 
So my code looks like this:
#define GPIO_DMA_SAMPLE_BUFFER (256)
uint16_t gGPIO_DMASampleBuffer[GPIO_DMA_SAMPLE_BUFFER] = {0};
void DMA_Init()
{
//Enable DMA clock
RCC->AHB1ENR |= RCC_AHB1ENR_GPDMA1EN | RCC_AHB1ENR_GPDMA2EN;
//Destination address increase, Source = Destination 16 bit wide
GPDMA1_Channel0->CTR1 = DMA_CTR1_DINC | DMA_CTR1_DDW_LOG2_0 | DMA_CTR1_SDW_LOG2_0;
//Request by tim2_upd_dma
GPDMA1_Channel0->CTR2 = 76;
//Transfer buffer size
GPDMA1_Channel0->CBR1 = GPIO_DMA_SAMPLE_BUFFER;
//Source GPIOC
GPDMA1_Channel0->CSAR = (uint32_t)&(GPIOC->IDR);
//Destination Sample buffer
GPDMA1_Channel0->CDAR = (uint32_t)gGPIO_DMASampleBuffer;
//Circular buffer mode
GPDMA1_Channel0->CLLR |= DMA_CLLR_UDA;
//Activate DMA1 Channel 1
GPDMA1_Channel0->CCR = DMA_CCR_HTIE | DMA_CCR_TCIE | DMA_CCR_EN;
NVIC_SetPriority(GPDMA1_Channel0_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 1, 0));
NVIC_EnableIRQ(GPDMA1_Channel0_IRQn);
}
void GPDMA1_Channel0_IRQHandler(void)
{
unsigned int statusOfInputDatalines;
extern uint16_t gGPIO_DMASampleBuffer[];
if (GPDMA1_Channel0->CSR & DMA_CSR_TCF)
{
GPDMA1_Channel0->CFCR = DMA_CFCR_TCF; //clear flag
for (int i = 128; i < 256; i++)
{
statusOfInputDatalines = (((gGPIO_DMASampleBuffer[i]) >> 6) & 0xFF); // reading status of the port C (6-13) pins
statusOfInputDatalines = (statusOfInputDatalines << 2) | ((statusOfInputDatalines >> 5) & 0x02) | ((statusOfInputDatalines >> 7) & 0x01); // reorder input pins
_SaveDataToBuffer(statusOfInputDatalines);
}
}
else if (GPDMA1_Channel0->CSR & DMA_CSR_HTF)
{
GPDMA1_Channel0->CFCR = DMA_CSR_HTF; //clear flag
for (int i = 0; i < 128; i++)
{
statusOfInputDatalines = (((gGPIO_DMASampleBuffer[i]) >> 6) & 0xFF); // reading status of the port C (6-13) pins
statusOfInputDatalines = (statusOfInputDatalines << 2) | ((statusOfInputDatalines >> 5) & 0x02) | ((statusOfInputDatalines >> 7) & 0x01); // reorder input pins
_SaveDataToBuffer(statusOfInputDatalines);
}
}
}