How many sections of RAM and Flash I can test with X-Cube STL package
Hi,
I'm working with X-Cube STL STM32CubeExpansion package, want to know how many sections of RAM and Flash I can test on STM32H745ZI MCU,
#define FLASH_SECTION_SIZE 1024U
#define RAM_SECTION_SIZE 128U
#ifdef STL_DISABLE_RAM_BCKUP_BUF
#define RAM_BACKUP_BUFFER_SIZE 0
#else
#define RAM_BACKUP_BUFFER_SIZE 32
#endif
#define TEST_RAM_START_ADDR (0x20000000U + RAM_BACKUP_BUFFER_SIZE)
#define TEST_ROM_START_ADDR 0x08000000U
#define TEST_FLASH_SECTION_NB 4 /* 4 Flash sections are tested */
#define TEST_RAM_SECTION_NB 8 /* 8 RAM sections are tested */
For Flash I can test 1024 which is 1MB of Flash I can test but my program is also running on RAM itself, how do I test complete RAM, any backup or threshold limit for RAM sections or regions of RAM able to Test,
Functional Safety team