How to calculate i2c timingR for stm32H5
I need help understanding how to calculate I2C timingR without using stm32cubemx.
I have searched high and low and I haven't had any luck finding solutions.
I want to create function that helps me manually setup the timing with different inputs without the use of stm32cubemx.
As of now i do a an i2c example working in standard mode, I am able to receive and transmit.
here are my settings: using i2c1

my clock configuration:

I would like instructions on how to get the timing above: 0x60808CD3
I have reviewed the Reference manual, but haven't had any luck with how it get's the values for SCLL, SCLH, SDADEL, and SCLDEL. Or the best rule of thumb with choosing the values.
here is the link to the RM: STM32H523/33xx, STM32H562/63xx, and STM32H573xx Arm<Sup>®</Sup>-based 32-bit MCUs - Reference manual
section 48 for ic2
Another question: SDADEL and SCLDEL does it calculate value every single time so on a different board (but with the same board) it might have a different value or would it be the same with the same chip.
Any help would be appreciated!
Thank you in Advance.