How to chose a pin compatible processor with larger RAM - STM32F756ZGT6 144-pin
Dear all,
Apologies if this is a naïve post.
I am trying to find a processor for the product that I am working on with larger RAM and FLASH but it must remain pin compatible to minimise code changes. The current processor is this "STM32F756ZGT6". With the current application its RAM is throttling at 100% and more features are still pending to be added. Therefore, if I can find another processor with the same pinout then the problem will be resolved.
Any help would be appreciated please?
Many thanks