How to configure PSSI to be used as Parallel Slave port
Hi,
I am currently using STM32H5 series, to transmit the RTC register content to an escalator base board. I need to transmit these data in a parallel manner (i.e. MCU act as a slave and the base board act as a master). I studied that STM32H5 series has PSSI which involves a data bus (PSSI_D[15:0]), data enable (PSSI_DE) and ready bit (PSSI_RDY) and a clock (PSSI_PDCK). Where the signal comes from the base boards are address and data lines (PMD<7:0>), chip select (PMCSx), read (PMRD) and write signal (PMWR).


A 4-bit address is transmit to the MCU (slave) from the base board (master). The MCU needs to place the data in the data bus as shown in the Figure 4-1. Is it possible to implement this in STM32H5 series? If not then suggests me some other STM MCUs with the following specifications:
1. Dimension between (5mmx5mm) to (9mmx9mm)
2. Pin count between 32 to 64
3. Package - Any package except ball grid array
Your help and advice much appreciated.