how to interface 50 pin lvds 1920*720 in f769-dis0
Hi ST-Members,
I need to interface a 10.3-inch LVDS display with a resolution of 1920x720 to an STM32F769-disc0. I also have an H743 Nucleo board. Could you please advise on the method I should use to make the display work? Additionally, I plan to initiate TouchGFX for an ECG application.
I came across a schematic for an interface board(attached below) from STM32F769-EVL to LVDS in the community. How can I follow this schematic to make it compatible with the F7-DISC0 or H7 Nucleo boards? Alternatively, is there an interface converter board available in the market that converts onboard MIPI DSI to LVDS? If not, please guide me on the proper steps to modify the PCB schematic for the STM32F7-DISC0 or H7.
Solved: LTDC (RGB) to LVDS interface - STMicroelectronics Community
regards,
embed_engr