Question
How to precisely control GPIO pulse width using instruction cycles?
The STM32F429 processor operates at 180MHz, with a clock cycle of 5.56ns. Can we generate pulses with a width granularity of 5.56ns using only ARM instruction delays?
For example: 5.56ns, 11.12ns, 16.68ns, 22.24ns?
In practice, I have encountered difficulties achieving the above operations, and I suspect that the pipeline affects the intuitive control of pulse width.
The following code controls the pulse width of PF0 output, the width = 'w':
```c
GPIOF->BSRR = 0x00000001; // PF0 output High
GPIOF->BSRR = 0x00010000; // PF0 output Low
```
Without considering the 3-stage instruction pipeline, the pulse width obtained would be 'w + 5.56ns':
```c
GPIOF->BSRR = 0x00000001; // PF0 output High
asm("nop"); // w + 5.56ns
GPIOF->BSRR = 0x00010000; // PF0 output Low
```
Similarly, by adding more `nop` instructions, we can achieve different pulse widths:
```c
GPIOF->BSRR = 0x00000001; // PF0 output High
// asm("nop"); // w + 5.56ns
asm("nop"); asm("nop"); // w + 11.12ns
// asm("nop"); asm("nop"); asm("nop"); // w + 16.68ns
GPIOF->BSRR = 0x00010000; // PF0 output Low
```
However, in practice, I have had to rely on an oscilloscope to adjust the pulse width,
the code lacks readability.
I am unsure whether adding 5.56ns requires 1 `nop` instruction or 2-3 `nop` instructions.
```c
__disable_irq();
GPIOF->BSRR = 0x00000001; // PF0 output High
asm("nop"); // w + 5.56ns
// asm("nop"); asm("nop"); asm("nop"); asm("nop"); // w + 11.12ns
// asm("nop"); asm("nop"); asm("nop"); asm("nop"); asm("nop"); asm("nop"); // w + 16.68ns
GPIOF->BSRR = 0x00010000; // PF0 output Low
__enable_irq();
```
When I copy the above code to another location, I have to modify it to achieve the same effect:
```c
__disable_irq();
GPIOF->BSRR = 0x00000001; // PF0 output High
asm("nop"); asm("nop"); // w + 5.56ns
// asm("nop"); asm("nop"); asm("nop"); asm("nop"); asm("nop"); // w + 11.12ns
// asm("nop"); asm("nop"); asm("nop"); asm("Question:
```
============================================================
1. What is the reason for the phenomenon described above?
2. Are there any remedies?
============================================================
The observed phenomenon is likely caused by the 3-stage instruction pipeline.
Instructions like `ISB` , `DMB` or `DSB` is can be used to achieve pipeline flush or clear ?
```c
__disable_irq();
__TODO_clear_pipeline__(); // how to do that
GPIOF->BSRR = 0x00000001; // PF0 output High
asm("nop"); asm("nop"); // w + 5.56ns
// asm("nop"); asm("nop"); asm("nop"); asm("nop"); asm("nop"); // w + 11.12ns
// asm("nop"); asm("nop"); asm("nop"); asm("nop"); asm("nop"); asm("nop"); asm("nop"); // w + 16.68ns
GPIOF->BSRR = 0x00010000; // PF0 output Low
__enable_irq();
```