Question
How to Properly Implement a Lookup Table for a Unipolar Sine Wave Inverter?
I'm designing a unipolar sine wave inverter using a lookup table to generate PWM signals, but I'm encountering some issues and have a few questions:
- Should the values in the lookup table start from zero, or from the peak value of the sine wave?
- Is it sufficient to create the lookup table for only half of the sine wave cycle (0 to 180 degrees)? After generating the first half-cycle, can I simply change the polarity to complete the full cycle, or is there another method I should follow?
- How should I handle the transition between the first and second half-cycles? Should I invert the polarity of the PWM signal, or do I need to modify the lookup table values?
- Could someone provide a small example of a lookup table for a unipolar sine wave inverter, and explain how to use it across a full cycle?
- I'm able to generate a sine wave without using complementary channels, but when I try to use complementary outputs on two channels, it doesn't work correctly. What could be causing this issue, and how can I fix it?
I'm struggling with these concepts, and any guidance or examples would be greatly appreciated. Thank you!