How to run program on STM32N6 after flashing without changing BOOT-1 jumper
Hello ST Community,
I’m working with the STM32 Nucleo-N657 board and need a way to execute my application after flashing to external memory without manually toggling the BOOT1 jumper on the board.
What I’m Doing Now:
- BOOT1 jumper is set to HIGH for development (DEV boot mode)
- I have a simple LED blink application built with GPIO configured in the FSBL context
- The code runs as expected in DEV mode (debug mode of STM32CubeIDE)
- I then flashed the signed binary in external memory using STM32CubeProgrammer and External Memory loader for Nucleo-N6 board at address 0x70000000.
- Then, I switched BOOT-1 jumper to LOW and reset the board. The code runs as expected from external memory.
Problem:
I have N6 board connected to a remote PC and won’t always have physical access to toggle the BOOT1 jumper and press reset.
I would like to know:
Is there a programmatic or configuration-based way to run the program automatically after flashing, without needing to change the BOOT1 jumper manually?
- Can this be achieved via STM32_Programmer_CLI, or by modifying BOOTROM-related OTP settings.
I am looking for a way to avoid all manual interventions between flashing and execution.
Any help or guidance will be greatly appreciated!
Thanks,