Skip to main content
Visitor II
July 31, 2024
Question

How to run STM32H735 CPU in maximum frequency

  • July 31, 2024
  • 1 reply
  • 788 views

I am trying to run STM32H735 in 550 MHz, i had read the reference manual so write the following code.

FLASH_OPTKEYR = 0x08192A3B;
FLASH_OPTKEYR = 0x4C5D6E7F;
if (SYSTICK_FREQ > 450 * 1e6 && !(FLASH_OPTSR2_CUR &= FLASH_OPTSR2_CPUFREQ_BOOST)) {
 FLASH_OPTSR2_PRG |= FLASH_OPTSR2_CPUFREQ_BOOST;
} else if (SYSTICK_FREQ <= 450 * 1e6 && (FLASH_OPTSR2_CUR &= FLASH_OPTSR2_CPUFREQ_BOOST)) {
 FLASH_OPTSR2_PRG &= ~FLASH_OPTSR2_CPUFREQ_BOOST;
}
while (FLASH_SR &= FLASH_SR_BSY)
FLASH_OPTCR |= FLASH_OPTCR_OPTSTRT;
while (FLASH_SR &= FLASH_SR_BSY)
FLASH_OPTCR |= FLASH_OPTCR_OPTLOCK;

And print the log output to monitor the register status

LOGF("SYSCFG - CPU_BOOST : %d, FLASH - CPU_BOOST : %d\n", SYSCFG_UR(18) & 1, FLASH_OPTSR2_CUR);

Here is the result
SYSCFG - CPU_BOOST : 0, FLASH - CPU_BOOST : 4

I expected that SYSCFG18::CPU_FREQ_BOOST should be set to 1, but it not.
Is there any process wrong or less for enable CPU_FREQ_BOOST bit?

    This topic has been closed for replies.

    1 reply

    Roy_HuangAuthor
    Visitor II
    July 31, 2024

    Problem solve,

    After enable RCC_SYSCFG, CPU_FREQ_BOOST turns to 1.
    SYSCFG - CPU_BOOST : 1, FLASH - CPU_BOOST : 4