How to update the program by USB DFU bootloader in system flash?
Hi there,
I am verifying the USB DFU bootloader in STM32F429BI.
I can normally enter the bootloader and connect my MCU using stm32CubeProg.
I can succeed in the program flash when I check the "Full Chip erase" option, otherwise, it will fail sometimes(see the LOG in the attachment)!

But if "Full Chip erase", it needs a bit long time. Can I erase the sector when needed only?
One more, each time I flash the program, I must reset the MCU by hand, can I set the MCU to auto-reset after download?
Thanks for your help.
My code as below:
#define BOOTLOADER_ADDRESS (0x1FFF0000)
#define BOOTLOADER_FLAG_VALUE 0xDEADBEEF
#define BOOTLOADER_FLAG_OFFSET 0x50
typedef void (*pFunction)(void);
uint32_t endstack = 0x20030000;
uint32_t *bootloader_flag;
uint32_t JumpAddress;
pFunction JumpToBootLoader;
int main(void)
{
bootloader_flag = (uint32_t*)(endstack - BOOTLOADER_FLAG_OFFSET);
if(*bootloader_flag == BOOTLOADER_FLAG_VALUE) {
*bootloader_flag = 0;
__HAL_SYSCFG_REMAPMEMORY_SYSTEMFLASH();
JumpAddress = *(__IO uint32_t*)(BOOTLOADER_ADDRESS + 4);
JumpToBootLoader = (pFunction)JumpAddress;
__set_MSP(*(__IO uint32_t*)BOOTLOADER_ADDRESS);
JumpToBootLoader();
} else {
*bootloader_flag = 0x1234ABCD;
}
HAL_Init();
SystemClock_Config();
LOG_INIT();
LOG_DBG("\n\nSTM32V6 USB DFU BootLoader test flag[0x%08x]...\n", *bootloader_flag);
MX_GPIO_Init();
MX_USART1_UART_Init();
HAL_UART_Transmit(&huart1, (uint8_t*)"send 0x5A to update...\r\n", strlen("send 0x5A to update...\r\n"), 100);
uint8_t rxBuf[10];
while (1)
{
HAL_Delay(1000);
LOG_DBG("DELAY 1s\n"); // hex1
//LOG_DBG("delay 1s\n"); // hex2
HAL_UART_Receive(&huart1, rxBuf, 1, 20);
if(rxBuf[0] == 0x5A) {
*bootloader_flag = BOOTLOADER_FLAG_VALUE;
LOG_DBG("Jump to BootLoader, flag[0x%08x]...\n", *bootloader_flag);
HAL_Delay(100);
__disable_irq();
HAL_NVIC_SystemReset();
}
}
}