How to use external reference voltage for ADC (Nucleo-H723ZG)
I want to provide external reference voltage to 16-bit ADC.

So i need to remove the R36.

And Vref is connected to Vref+ pin on the board.
These two things are the only steps i need to do right, after that i have to connect my external source to the vref+ pin and it will be the reference voltage for my ADC.

And i need to make sure Vref<= Vdda, small increase might not be an issue right? Are there anything else i need to look into