HRTIM1 Starting the Master Timer or any other Timer with External Events
Hello,
In my project five high resolution timers should start on the SYNC signal. They go HIGH on the COMP1 value 32 until an External Event Signal comes and sets the output LOW. The counters reset and get triggered with the next SYNC Signal.
The sixth timer (or the Master Timer) must start with the External Event Signal.
It is essential that the timer starts with the EEV and not just be inverted on the output. It is necessary to later link the inactive state change of the first five timers to the compere registers of the sixth timer. In the end I can set five timers HIGH at once but set them LOW at different times and delays with respect to the EEV.
Is it possible to configure this in MX / IDE?
I'm using a NUCLEO-G474RE Board.