HSE Bypass mode - Possible use of OSC_OUT as GPIO
Hi I am looking into using STM32F446RCTx for my design, which includes 2 x USB FS 2.0 (1 x Host + 1 x Device). Hence need to provide an external HSE. I want to use an Oscillator, meaning I setup the HSE as "Bypass Clock Source" .
With this setup I planned to use the pin 6 (PH1_OSC_OUT) as a GPIO for other functionalities. But the STM32CubeMX setting does not let me do this.
I see that this pin will be (OSC_OUT) High Impedance as per RM0390 - Page 120. Am I right in say that I MUST leave this pin NC and cannot free up to use as GPIO?
Thanks.