HSE crystal dead
Hello
I am trying to powerup external 8MHZ crystal on STM32F407VET6 MCU but it is completely dead. I run the LED bliking program using HSI, and it is working sucussfully. Boot 0 and Boot1 pins have been PD with 500 ohm.
I also run the same code to use HSE on STM4 Discovery board after removing R68, I see HSE on board is working.
Below are my caclulation
Frequency = 8 Mhz,
Co = 7 pF ( as per datasheet)
CL= 10 pF ( as per datasheet, used 20pF CL1 and CL2)
ESR = 100 ohm ( as per data sheet)
After calculation gmcrit comes..
gmcrit = .287
gm = 5 ( from ST data sheet)
gain margin = 5/.287 = 17
so gain margin > 5 condition is met.
I also changed Rext to 0, 100, 200, 500 , 1000 ohm. HSE is dead.
PCB design seems ok , and I assume for now no issue with PCB design.
I have gone through AN2867, but not sure what point I am missing.
Kindly suggest where could be the fault. I eliminate software issue as same code is making HSE work on Discovery board.