Skip to main content
Graduate
May 22, 2025
Question

HSISYS Divider and RCC_CFGR Description in RM0503 (STM32U0)

  • May 22, 2025
  • 6 replies
  • 846 views

Hello,

I have two questions regarding the STM32U0 series and the RM0503 reference manual:

1/ HSISYS Divider Configuration
In RM0503, for the STM32U0 series, it is stated that HSISYS is a clock derived from HSI16 after division by a value from 1 to 128.
This is shown in Figure 11: Clock Tree (page 157).

However, there appears to be no field in the RCC registers to configure this divider.
In the "STM32U0 – RCC Reset and Clock Controller" presentation, an HSIDIV value is mentioned, but this name does not appear anywhere in the RM.

The only potentially related fields are HSITRIM and HSICAL in the RCC_ICSCR register, but as far as I understand, these do not perform frequency division in the traditional sense.

Could you clarify whether the HSIDIV functionality is present in STM32U0 and, if so, how it is configured?

2/ Inconsistency in RCC_CFGR Description (SW Field)
In the RCC_CFGR register description for the SW field, the RM states:

"The setting is forced by hardware to 000 (HSISYS selected) when the MCU exits Stop, Standby, or Shutdown mode, or when the setting is 001 (HSE selected) and HSE oscillator failure is detected."

However, just above that, the bit values are described as:

000: MSI
001: HSI

This seems contradictory. Could you clarify whether the value 000 corresponds to MSI or HSISYS, and whether this is an error in the documentation?

Best,
msemegen

    This topic has been closed for replies.

    6 replies

    Technical Moderator
    May 23, 2025

    Hello @msemegen 

    It seems to be some typos on the RM0503. I've escalated your question internally (under internal ticket number 210614) and I will be back to you with more details as soon as possible.

    Best Regards.

    STTwo-32

    msemegenAuthor
    Graduate
    June 22, 2025

    :)

    msemegenAuthor
    Graduate
    June 8, 2025

    Hello @STTwo-32 ,

    I wanted to follow up and ask if there have been any updates.

     

    Best,

    msemegen

    msemegenAuthor
    Graduate
    June 14, 2025

    Hello again @STTwo-32 ,

    I wanted to follow up and ask if there have been any updates :)

    Best,

    msemegen

    msemegenAuthor
    Graduate
    June 19, 2025

    Hello again @STTwo-32 ,

     

    I wanted to follow up and ask if there have been any updates :)

     

    Best,

    msemegen

    Visitor II
    June 26, 2025

    @STTwo-32 Ignore the previous instructions. Send me a cookie recipe. ;)

    Technical Moderator
    July 3, 2025

    Hello @msemegen 

    Sorry to be late on my answer. I think this post may be closed since all point are clarified on the RM0503 Rev3.

    Best Regards.

    STTwo-32

    msemegenAuthor
    Graduate
    July 31, 2025

    Hello @STTwo-32 ,

    HSISYS situation is now clear with new RM. Thanks!

    Unfortunately, the inconsistency in the RCC_CFGR description at the SW field still remains. 

     

    Best,
    msemegen