I can't connect my Nucleo to my STM32L0 board
Well, I'm new to the STM32. I'm developing vibration and temperature sensors, which used to be equipped with an atmega.
With the new demand for processing I decided to upgrade by putting an STM32L0 in place of the old controller.
The problem is that now I can't use my CUBE Programmer to connect to my board via Nucleo's STM Link.
An error message appears whenever I click Connect, and my Nucleo board flashes red.
I think I may have made a connection or PCB design error.
Information:
My system has 1 accelerometer 1 temperature sensor 1 Lora radio 1 battery sensor and a 3v3 regulator.
The clock has been set to 25KHz by means of an Oscillator Crystal.
and the BOOT0 pin is not connected to anything other than the pull-down resistor.