I have a problem of using SPI in STM32H753VIT6 CHIP
Hello,
I'm trying to do SPI communication with an ADE1201 chip through an STM32H753VIT6 chip.
The maximum allowed frequency of the ADE1201 is 10MHZ, so I set the SPI to communicate with the MCU at 6.25MHZ.
(The clock for SPI communication is 25MHZ, and I set the PRESCALER value to 4).
However, a strange phenomenon was observed.

I observed through the scope that the SPI CS signal should be 0 continuously, but it turns to 1 in the middle.(See attached photo).
However, if I set the PRESCALER value to 8, the CS signal is continuously output as 0.
What could be the cause? And how can I solve this?
Could this be due to the usage of HAL_SPI_TransmitReceive function?